Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Hi ;I am having a confussion on how to set the interrupt priority of a desired peripheral . I am using IAR IDE version 3.11.1 and the MCU is STM8S103F3F6 . I need to know which interrupt table IRQ number I should take account to configure the interr...
Function ADC2_ConversionConfig do three steps:sets ADC result alignenable/disable continuous conversion (there will be problem, unrelated to Continuous mode)writes desired channel into ADC2->CSR (there will be another problem)but if that function is ...
Hello EveryoneI use STM8L001J3P6 in my project. I want to use timer 3 on compare mode but I dont write any value timer3 register. I write 129 (TIM3_CR1=129;) but register value is zero. Anyone can solve this problem?Thanks.
Hi. I'm using the STVD IDE with Cosmic with an STM8TL52F4 MCU with the 'Minimize Code Size' compiler option selected. Under Debug instrument->ICD MCU configuration->Options, I set the DATASIZE_bit6 Value to 1 (the other DATASIZE bits are 0) and made ...
Hi. I am trying to design an NFC antenna for a two layer pcb. I have done this before using the eDesignSuite tool but can no longer see the dropdown to choose more than one layer. Have I missed something obvious or has this feature been removed? Than...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.