2022-05-11 2:40 AM
Hello,
I am developing a project with STM8L050J3 microcontroller using Evaluation Board STM8-S08-DISCO and STVD version 4.3.12.
I need to calibrate the internal HSI oscillator, but for some reason that I have not been able to identify, although I compile without any error when I run the program, at the CLK_AdjustHSICalibrationValue(HSI_Calibration_Value); instruction I get the error: swim error (30007): swim communication error and then : "Error: gdi-error [40127]: flash memory not accessible while core is
running" (see attached screenshots).
Is this a limitation of the debugger, or do I make some error in using the calibration instruction?
Thank you for any response you may have
Sisto
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.