2022-05-04 10:58 AM
$ sdcc -mstm8 --out-fmt-elf -o build/firmware.elf build/{main.rel,uart3.rel,misc.rel}
?ASlink-Warning-Undefined Global 'null' referenced by module 'main'
What is meaning?
Module "main.rel" was compile without errors/warning.stm8-gdb has segfault when i load this elf :(
2022-05-04 12:29 PM
Perhaps you have some object dumping tools, or you can look for correlating data in the .MAP or .LST files.
>>Module "main.rel" was compile without errors/warning.
You understand that means Very Little, simply that the code appears syntactically correct, not that it is functionally correct, or sufficient to get closure in the linker.
Perhaps use bi-section techniques to isolate the portion of code involved, or the delta from the last code that compiled and linked properly.
2022-05-05 12:27 AM
>Perhaps use bi-section techniques to isolate the portion of code involved, or the delta from the last code that compiled and linked properly.
yeah, i was figure out with it!
"static uint16_t tick=0"
using a static variable in the main loop broke the build project in ELF format
fixed it through replace to local variable. Thanks for answer!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.