2024-11-20 11:44 AM
After many years without problems, now my STVD is acting weird.
It shows different behaviors running as user and admin
The Open Workspace file selector pup-up file type is set to show only .exe files (it should be .stw files)
When I start debugging it compiles, hangs on Restoring context message on the small Loading... pop-up, after some seconds shows not responding on window title and crash. Note that the main windows title shows some GDI error message
The Open Workspace pop-up is ok
When I start debugging an error message pops-up "Connection error (usb://usb): gdi-error [40201]: can't access configuration database"
I've tried so far:
Hardware info:
Dell G3 laptop running Windows 10 22H2
STM8S003K3 MCU
ST-Link V2
COSMIC Compiler
Any help is very appreciated.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.