Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM8 assembler directives reference

Hi, I have look Extensively THREE different times now to find an assembler reference.  NOT the instruction set, the assembler directives.  Data types declared, conditional assembly (if avail), Everything the Assembler uses to generate machine code. I...

Resolved! Query about AN4070 Application Note

Hi,I have been trying to design a double stage single phase grid connected PV Microinverter system.I came across an Application Note AN4070, in which you have designed a 250W grid connected Microinverter. I tried to follow the procedure and design an...

RJ7044 by Associate
  • 1062 Views
  • 1 replies
  • 0 kudos

Resolved! NB-IoT board

Hello,I'm working on a project that requires the implementation of NB-IoT and to do this I started by testing the Discovery Kit B-L462CELL1, which is very poorly documented. I also noticed that the LBADXX1SC modem used by the kit is now obsolete.Can ...

celika by Associate
  • 1531 Views
  • 3 replies
  • 0 kudos

Resolved! STM8S003 Trying to save 4 parms in EEROM.

Need to IAP save two 16(10) bit ADC values to EEROM. Done parm saves before in STM8S105, but want to see it in ICP mode.In NXP MC9S08, I can turn off download, which cleared Its EEROM. That let me run the ADC "learn" of the values, save them to EEROM...

STUW81300 STWPLLSim

 Hello.I want to use STUW81300 to create 9 GHz with great phase noise.Reference: 50 MHzPDF:50MHzSingle-EndedSTWPLSim v5.3 was used for the loop filter design.However, the actual measurements were 3~7dB worse than the simulated values.All settings see...

hccho by Associate
  • 1307 Views
  • 1 replies
  • 0 kudos

Specs for EXTVCO_IN for STW81200

Both STuW81300 and STW81200 have the option of using an external VCO but the inputs characteristics aren't specified anywhere. What is the input frequency range, input power/sensitivity in dBm or 50ohm match for single-ended input? There is one appli...

mallets by Associate
  • 800 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.