2007-03-05 7:19 PM
2011-05-17 12:39 AM
Thank you for respons !
I will trie this as soon I can erase my flash ... Luc Vercruysse2011-05-17 12:39 AM
Used target = MCB-STR9 + µVision3.50 from Keil.
I tried to build the blinky example to boot and run in flash bank 1. In the ''STR910 Flash with CFG'', I changed, using the configuration wizard following items :FLASH MEMORY INTERFACE (in STR91x.s)
Flash bank 0 Enable = true
BBSize = 512KB
BBADD = 0x800000
Flash bank 1 enable = true
NBBSIZE = 32K
NBADDR = 0x00000 (<= remapped this on address 0 to boot)
CONFIGURATION (in STR91xCFG.s)
CSX (Chip select mapping) = true (<= switch boot sector)
The result is that the JTAG is blocked. I get the error 'could not stop ARM device'. Even erasing immediatly after reset is not possible. This is the second time this happens. The first time i did replace the STR9 device. Now I did order a RLINK device. I hope this works for erasing it ! My question : WHAT IS WRONG WITH ABOVE SETTINGS ? Thanks Luc
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.