2008-05-06 8:41 AM
2011-05-17 12:39 AM
Does anyone know if it is possible to use a UART receive interrupt to wake up the processor from sleep mode? Or should I just try to tie the UART transmission wire to some external interrupt pin elsewhere on the processor?
Thanks.2011-05-17 12:39 AM
Hi SJackson,
It's not possible to use UART receive interrupt to wake up the processor from sleep mode. In fact, sleep mode can be triggered by RTC Alarm, external interrupt via wake-up unit (WIU) or externel reset. with best regards, mirouWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.