Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Infinite ISR on STM8L

Posted on April 01, 2014 at 21:04I'm exploring an STM8L152 on the Discovery Board. That board has a user button, which I have set to trigger an interrupt on a GPIO (pin C1, if that matters). I can watch the interrupt fire in the debugger (using STVD...

vince by Associate III
  • 971 Views
  • 0 replies
  • 0 kudos

About STM8 decimal adjust

Posted on March 29, 2014 at 12:02Hello everyone, I just started learning STM8 assembly language, but can not find the decimal adjust instruction, so do not BCD arithmetic.Have thought about writing a decimal adjustment subroutine, the addition shoul...

ysc by Associate
  • 1495 Views
  • 2 replies
  • 0 kudos

STM8S103K3 - ADC takes longer than expected?

Posted on March 27, 2014 at 18:04I am timing the ADC conversion from TRGO to EOC.  I calculate that the conversion should take 3.5us but I measure a minimum of 4.0us using an oscilloscope.I have included the relevant code loop below.Please does anyo...

PM6680A based project simulation in eDesign Studio

Posted on March 27, 2014 at 14:531) After saving either locally or remotely the project, I can't find anymore my database added components. Could it be wanted or a bug? 2) PSpice export option is grayed, is it because ST PSpice Project Export Manage...

olmirko by Associate
  • 1420 Views
  • 1 replies
  • 0 kudos

Interrupt cant set global variable?

Posted on March 13, 2013 at 13:22Hi all. I got a problem: Every time i am setting a global variable in my ISR it is set to 0 after the ISR has ended!volatile int test; void main(void){ TIM1_DeInit();  TIM1_TimeBaseInit(10, TIM1_COUNTERMODE_UP, 20000...

texton1 by Associate II
  • 3649 Views
  • 6 replies
  • 0 kudos

how to access nand flash?

Posted on March 14, 2014 at 22:19Hi,I am use STR911 to access external NAND flash ST NAND08GW3B. Where can I find information to use STR911 EMI to write and read from NAND flash? Is there any NAND flash driver for ST NAND08GW3B I can download?Thanks...

jian by Associate
  • 1219 Views
  • 1 replies
  • 0 kudos

STM8L052 vs STM8L152

Posted on March 18, 2014 at 14:38i have made program for DiscoveryL152, with STM8L152. mcu. Program works properly. Now i try to start this program on other board with STM8L052C6 mcu. LCD not works - all COMx and segment pins are idle...... In all S...

ygrod by Associate II
  • 986 Views
  • 0 replies
  • 0 kudos

STM8L152-STM8L052 LCD

Posted on March 18, 2014 at 13:49i have made program for DiscoveryL152, with STM8L152. mcu. It works properly. Now i try to start this program on other board with STM8L052C6 mcu. LCD not works - all COMx and segment pins are idle...... In all ST doc...

ygrod by Associate II
  • 799 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.