2014-03-14 2:19 PM
Hi,
I am use STR911 to access external NAND flash ST NAND08GW3B. Where can I find information to use STR911 EMI to write and read from NAND flash? Is there any NAND flash driver for ST NAND08GW3B I can download?Thanks, Jian2014-03-19 9:29 PM
It's been a while since working on STR9 parts, but I think you need to refer to the documentation and schematics for your board. NAND parts act more like hard drives than memory, so you'll only see a few addresses, and data/command access, and ready signals.
For code examples for NAND devices, you might want to look at uboot/linux sources for generic code to identify and access the NAND devices. Other freely available NAND code may also be usable, you'd just have to define a handful of addresses used to access the parts. The FMI configuration would be a matter of chip selects (memory region), and signal timing, which would depend on the part's parameters, and the operational frequency of the STR9We’re moving the ST Community to a new platform to give you a better and more reliable community experience.