Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Windows XP remote desktop to Cosmic STM8

Posted on March 11, 2014 at 17:16Cosmic STM8 is installed in Windows XP with license. Since we are working in a networked-host, we will access such Windows XP host using Windows XP remote desktop access. When Cosmic STM8 is started from the physical...

scheung by Associate
  • 991 Views
  • 0 replies
  • 0 kudos

PSD854F2 PLD programming question

Posted on March 11, 2014 at 17:12Hello, I have recently had an issue with a PSD854F2 not controlling pin PA0 as a GPIO correctly. During troubleshooting we used PSDSoft Express to pull the image from the device. After programming a fresh image onto ...

kdevuyst by Associate
  • 1099 Views
  • 0 replies
  • 0 kudos

STM8S003F PD4 doesn't work as GPIO

Posted on February 27, 2014 at 14:44Hi all! I am using STM8S003F microcontroller with UART in async mode. I want to use UART1_CK pin as regular GPIO in push-pull mode. This pin is PD4. When peripherals are configured as below:    PD_DDR_DDR4 = 1;   ...

kiroid by Associate II
  • 3033 Views
  • 4 replies
  • 0 kudos

STM8S and EXTI and Continuous Interrupts

Posted on January 24, 2012 at 08:25MCU: STM8S105C6Port: GPIOBBit: 2 GPIOB:2 is the only pin/bit set up for external interrupt, yet regardless of any edge sensitivity setting in EXTI_CR1, once an interrupt is invoked it is continuously invoked while ...

Workalot by Associate III
  • 4251 Views
  • 6 replies
  • 1 kudos

E/H/L ockets of 24 bit address

Posted on February 20, 2014 at 14:13Hi all,I cannot find what the meaning is of those E/H/L parts of the address! Nowhere in the datasheets are the abbreviations explained. I presume H and L are the High and Low ockets but what is E?I don't understa...

albert1 by Associate
  • 1469 Views
  • 2 replies
  • 0 kudos

USB hardware with STM8 - library

Posted on November 10, 2013 at 19:22 Hello, Is there any software library that allows to build USB hardware with STM8 microcontroller without any additional chip? I am looking it but I have not found anything so far. Such library would greatly impro...

Float data doesn't make sense

Posted on February 28, 2014 at 12:07I set a floating-point (*data) , (*data) = (*data)/(pow(10,Strlen-3-DotPos)),(*data)=1234,pow(10,Strlen-3-DotPos)=100, the result was 12.33999 how did that happen? And I want to get an aprecise result 12.34.  How ...

0690X00000602jWQAQ.jpg 0690X00000602jbQAA.jpg 0690X00000602jlQAA.jpg

ST7580 Maximum Devices on the Power Line

Posted on September 19, 2013 at 22:50I need to transmit to about 500 receivers, each one needing ~1.5kbps of data.  So I need ~750kbps of total bandwidth.  Can I use one transmitter per 5 receivers so that I have enough bandwidth (1.5k*5 = 7.5kbps w...

Software USB on STM8S

Posted on February 22, 2014 at 14:34I wrote a program receiving and transmitting data to the microcontroller STM8 (Tested on STM8S103F3)But so far not implemented in full support of the protocol itself USB :( Source code and description in Russian ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.