2014-03-27 6:53 AM
1) After saving either locally or remotely the project, I can't find anymore my database added components. Could it be wanted or a bug?
2) PSpice export option is grayed, is it because ST PSpice Project Export Manager isn't installed yet, or the PM6680A PSpice export is not supported yet? 3)The resistor divider proposed for undervoltage function looks unrealistic (100K hr, 1.47M lr for a 19 to 30V input range)... Thanks in advance2014-03-27 7:57 AM
Dear Sir.
first of all let me thank you for your interest on our products (you made the right choise) and for submitting your issues on this forum.
About the issues you are facing:
1) it is a wanted feature: after the save, the added components are mantained only at schematic level and not maintained at database level. I have to admit that this behavior could result annoying so we are going to add this change request.2) It is because ''PSpice export'' for PM6680A solutions is not yet supported.
3) Yes it is strange. We will add an item to our bug tracking system.
We will update this post as soon those issues will be fixed and made available.
Best Regards and thank you again.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.