Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Develop STM8L on Discovery Board?

Posted on August 02, 2013 at 10:48I've got an STM8L Discovery board, but I've decided to use the STM8L101 chip. Is this chip a subset of the STM8L152C6T6 used on the didcovery board? Does the swim use the same IO port/pins on both chips? Or do I nee...

STR711FR2 USB Virtual Com Port IAR *HELP* needed.

Posted on April 08, 2014 at 14:00Hi,I have been looking at implementing USB VCP on a STR711FR2. I have downloaded the str71x demos from ST. I have built the project and got it running but when I plug into the USB port I get �Unknown Device� The boar...

simon2399 by Associate II
  • 1695 Views
  • 2 replies
  • 0 kudos

Use SDCC in STVD

Posted on April 15, 2014 at 11:50Hi, I wanted to integrate the free SDCC Compiler in STVD. But I can´t find a possibility to add a new toolset. If I install Raisonance, a new entry in the toolset dropbox is generated. So there must be a possibility ...

nikolas by Associate
  • 1052 Views
  • 0 replies
  • 0 kudos

USB, one more time...

Posted on June 05, 2012 at 15:19Hi there, I try to use the Virtual Com Port sample for str71x coming with um0290 package. It is said in the documentation that I should ''Indicate to the PC the location of the stmcdc.inf file (already provided in the...

STR711FR2 USB Virtual Com Port IAR *HELP* needed.

Posted on April 04, 2014 at 13:34Hi,I have been looking at implementing USB VCP on a STR711FR2. I have downloaded the str71x demos from ST. I have built the project and got it running but when I plug into the USB port I get “Unknown Device�? The boa...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.