difference between ST10F276, ST10F276E and ST10F276Z5?
Posted on December 05, 2015 at 16:45What is the difference between the 3 variants?
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Posted on December 05, 2015 at 16:45What is the difference between the 3 variants?
Posted on December 05, 2015 at 10:29Hi, I'm using STM8S003F3 controller to monitor a temperature sensor using I2C Interface. I'm able to monitor while in debug and Run mode (in STVD IDE) using SWIM, but once I program into flash (using STVP through ...
Posted on December 03, 2015 at 12:29I m beginer to tis stm8s i m using stm8s003 series with cosmic compiler to develop a product i need a sample of tm1638 interfacing with spi can any one help me please .. thanx in advance .. #stm8s
Posted on December 03, 2015 at 10:14I bought the starter kit STEVAL-ISB027V1, EWSTM8-2015 I downloaded and installed it but I can not find the source of the firmware.Where are? Thanks.
Posted on November 30, 2015 at 10:22Hi, I am implementing SWIM Protocol for an own programmer. It already works quite well with STM8S003 but I am facing difficulties with STM8L101. I wonder why the 128 HSI-timing-pulse on SWIM entry from the STM8L i...
Posted on November 25, 2015 at 15:14Hello everybody, I'm working on the STM8 discovery board to implement some application which controls the STM8's GPIOs from an SPI master. The code relies on SPI interrupts. I would like the master sends the addr...
Posted on January 29, 2015 at 08:58Let the stm8s003k3 i2c slave,Works fine, butWhen the master send general call address(0x00), stm8s003k3 stops,Of course, I2C_GeneralCallCmd(TRUE) is called.and the EVENTI2C_EVENT_SLAVE_GENERALCALLADDRESS_MATCHEDis ...
Posted on November 20, 2015 at 10:00Hi!I have to generate a PWM that must be quite closely synced to an external signal of 50 Hz (to avoid any drifts).From the documentation contents of STM8S008F/K of it using the TIM1 external trigger (ETR) to res...
Posted on November 18, 2015 at 12:34Thank you Luca, As per your reply we already change the workspace toolset Rootpath as follows: ''C:\Program Files\COSMIC\32K_Compilers\CXSTM8''but I can't understand the meaning of- your linker file specifi...
Posted on December 17, 2013 at 14:31Hello everyone. I am making Kitchen Clock on STM8S105C6 and STM8 touch sence library. I need 4 buttons and i have configurate them as SCKEY. Now they works fine. My problem is that library catch only one button a...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.