Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

pre-build command in STVD

Posted on December 17, 2015 at 20:10Is there any way to execute a ''pre-build command'' in STVD? I would like to auto-increment a version number in the source-code prior to each build. I have a command-line utility that modifies a header file to do ...

dporter by Associate
  • 746 Views
  • 0 replies
  • 1 kudos

STM8 checksum

Posted on December 16, 2015 at 15:44Hi,i have generated hex file for a particular project. The controller used is stm8s003f3. My question is regarding checksum. I'm not familiar with checksum. How can i add checksum to this hex file.? How can i dete...

Design calculation (Application note)

Posted on December 16, 2015 at 11:23HI, I have designed a isolated flyback using VIPER37LD in eDesign Studio and found the schematic is matching with the expected.but i want to conform the components value through design calculation.so i request you...

raju by Associate
  • 1148 Views
  • 0 replies
  • 0 kudos

STM8L Discovery

Posted on December 08, 2015 at 20:26Hi guys,I am trying to access STM8L Discovery board bootloader, to upload some code..The problem is...where can I connect my usb/rs232 converter??The pins for usart1 are connected to LCD display..Does any one know...

lmx1 by Associate II
  • 1374 Views
  • 1 replies
  • 0 kudos

RTC problem

Posted on November 19, 2015 at 23:22I'm working on some code to set the RTC alarm, and I've gone through all the resources I can find on how to set this up correctly, but it's just not working. If you could take a look and see if I've missed anythin...

jherrmann by Associate II
  • 2877 Views
  • 2 replies
  • 0 kudos

zero page ram page memory mapping on STM8S003

Posted on December 09, 2015 at 10:21Hello,on STM8S003F3U according to datasheet there is 1024(total ram) - 513(stack) = 510 bytes for user application: 256 byte in the zero page and (510-256)= 254 in Ram section.If use the short stack compilation op...

''C'' Library for ATmega8 and ST7590 Modem PLC

Posted on December 07, 2015 at 20:15For a project in prototype assembly stage it is necessary to link an 8-bit microcontroller with the modem ST7590T, for it would be desirable to have the ''C'' library that is mentioned in the 1076 User Manual (UM1...

C Library for ATmega8 to drive ST7590

Posted on December 07, 2015 at 20:10For a project in prototype assembly stage it is necessary to link an 8-bit microcontroller (ATmega8) with the modem ST7590T, for it would be desirable to have the ''C'' library that is mentioned in the 1076 User M...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.