2015-11-25 6:14 AM
Hello everybody, I'm working on the STM8 discovery board to implement some application which controls the STM8's GPIOs from an SPI master.
The code relies on SPI interrupts. I would like the master sends the address of the targeted register (15 bits) and a 16th one (MSB) which indicates the access mode (Read or Write). I can't solve an issue about pointers. The interrupt code is the following : &sharpdefine ACCESS_BIT 7 &sharpdefine READ_INPUT_ID 0x50 char cpt, temp, add; uint8_t mode_add_MSB, add_LSB; bool access; // '1' = W, '0' = R INTERRUPT_HANDLER(SPI_IRQHandler, 10) { if (SPI_GetITStatus(SPI_IT_RXNE)!=RESET) { if(cpt==0) // Reception of the access mode bit and the 7 MSB address bits { while(SPI_GetFlagStatus(SPI_FLAG_RXNE)!=SET); mode_add_MSB = SPI->DR; access = mode_add_MSB>>ACCESS_BIT; // Insulation of the access bit mode_add_MSB&=~(1<<ACCESS_BIT); // Ignorance of the access bit in the MSB address bits cpt++; SPI->DR=cpt; // debug } if(cpt==1) // Reception of the LSB address bits { while(SPI_GetFlagStatus(SPI_FLAG_RXNE)!=SET); add_LSB = SPI->DR; cpt++; add=((mode_add_MSB<<8)|add_LSB)&add_LSB; // Concatenation of the 15 bit register address if(access==READ_MODE) { temp = (uint8_t *) add; // error line 249 : I would like to affect in temp the content of the memory case which address is add. SPI->DR=temp; } } } } Can anybody can help me please ? Let me know if it's not clear Thank you The interrupt code is not complete yet but I have yet a problem with the targetting of the register. I would like to send, from the master, the address of the IDR register for the port targetted and read it. I got the following error code with Cosmic &sharperror cpstm8 ..\..\src\stm8s_it.c:249(23+3) incompatible pointer assignment #stm8-pointer-language-c-address2015-11-25 8:05 AM
Hello,
you seem to have some confusion about 8 bit types, 16 bit types and pointers. In your code, all variables are 8 bit, and that is probably not what you want, because you try to store a 16 bit value (the address) into at least onr of them (add).. Coming to the specific error you mention, you write temp = (uint8_t *) add; The compiler understands the following: take add (a char variable), cast it to a pointer to char (so it is now an address pointing to a char), and assign it to temp (another char variable). That makes char = pointer, which is forbidden in C. If you want to store into temp the value at the address pointed by add, you can write temp = *(uint8_t *) add; that will compile but I'm not sure it will do what you expect, since the address you get is always lower that 0xFF. The standard way to access a char variable in the whole STM8 memory space is char * address; char data; address = (char *)0x200; // or any other value, fixed or coming from a calculation data = *address; Hope it helps.2015-11-27 1:49 AM
Hi luca, thanks for your answer.
It helps yes, because I didn't know that we have to cast a value before affect it into a pointer. I was trying all writable syntax, but not the good one ^^ The concept of pointer is not easy for me, but it seems very usefull. Now it works. Thank you :DWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.