2015-11-30 1:22 AM
Hi,
I am implementing SWIM Protocol for an own programmer. It already works quite well with STM8S003 but I am facing difficulties with STM8L101. I wonder why the 128 HSI-timing-pulse on SWIM entry from the STM8L is ~85us long (I would expect 64us). I wonder if this is because the HSIT bit in SWIM_CSR is not set during reset and the hsi is not calibrated before OPT loading. Does the STM8L trim the HSI after reset-release (which includes OPT-loading) and therefore change the SWIM-clock speed? So do I need to recalibrate my SWIM timing after stm8 option bytes have been loaded by cpu after reset-release? My STM8S005 show similar behaviour. The STM8S003 I have tested are older production and STM8L und STM8S005 are ''fresh''. I did not check the issue on new STM8S003 yet - maybe it is similar..? Thanks & best regards, Alex #swimWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.