Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problems with jp instruction

Posted on February 26, 2016 at 10:04We are using assembler code in our C-code. The jp instruction is used to jump into the booloader. But sporadic the jp instruction is not working. We have also used jpf instruction. Without success. What can be the...

Cannot compile with Cosmic

Posted on February 26, 2016 at 03:21Hi,I'm trying to use the Cosmic 32K compiler in ST Visual develop and having created a completely new project with no additional code in, I can't compile it. I can't compile using Idea either.My error is:&sharperr...

harris by Associate II
  • 1486 Views
  • 1 replies
  • 0 kudos

ADC CONTINUOUS conversion Problem.

Posted on February 25, 2016 at 13:10I below code, I am reading ADC counts and sending it over CAN. ADC is working properly for _SINGLE conversion mode.... But it is not working for CONTINUOUS Conversion mode mode.

STM8 LIN driver suit and lingen utility

Posted on February 23, 2016 at 12:22 We are using the LIN Driver suit V 5.1.0 from ST microelectronics. The demo project provided in that is having a lin_basic_demo.ldf and lin_basic_demo.lgn files. I was successfully able to regenerate lin_cfg.c, l...

Issue with ST1CC40 in eDesign Studio

Posted on February 17, 2016 at 18:49I'm trying to design a constant current driver in eDesign Studio using the ST1CC40DR chip. I've set my output requirements to 4.8V and 1.2A and the input is 12V DC. With a 2% LED ripple current and 10% inductor ri...

Problem with the DMA datacounter of stm8l051

Posted on February 18, 2016 at 05:02Hi,I'm using DMA to transfer the data from USART1,The length of the data is varible.So I open the USART IDLE LINE interrupt.I try to set the DMA data counter to zero by using the function ''DMA_SetCurrDataCounter(...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.