2016-02-25 6:21 PM
Hi,
I'm trying to use the Cosmic 32K compiler in ST Visual develop and having created a completely new project with no additional code in, I can't compile it. I can't compile using Idea either.My error is:&sharperror cpstm8 C:\Program Files (x86)\COSMIC\32K_Compilers\CXSTM8\Hstm8\mods0.h:1 FlexLM No such feature exists.main.c: The command: ''cxstm8 +debug -pxp -no -l +mods0 -pp -i''C:\Program Files (x86)\COSMIC\32K_Compilers\CXSTM8\Hstm8'' -clDebug\ -coDebug\ main.c '' has failed, the returned value is: 1exit code=1.Could anybody advise me on how to solve this?Thanks, #stm8 #stvd #compiler #cosmic2016-02-26 12:57 AM
Hello,
the error message means the compiler cannot find the license it needs. Possible causes are - you did not copy to the /lic directory the license file sent by Cosmic - you have more than one Cosmic stm8 compiler installed on your computer. Hope it helps. Regards, LucaWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.