2016-02-18 1:16 AM
Can I use only one HV power source (HVM or HVP)? I need pulses single polarity.
#sthv800-single-polarity-hv2016-03-03 12:47 AM
Hello Serghei,
Yes, you can, for instance if you need only HVP, the suggestion is to connect anyway the negative voltage supplies, namely: - HVM=HVM_CW= 0V (or -3V) - VDDM= -3V (mandatory) If you have to use only HVM, do connect anyway HVP=HVP_CW=0V (or +3V) and VDDP= +3V (mandatory) Please, for further support contact directly ST prod. team in division thru my person:mailto:antonio.ricciardo@st.com
, so in this way we can share additional details about your prj Regards AntonioWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.