Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-Link V2 STM8S Program Problem

Posted on June 20, 2016 at 13:23Hai,    I have write code for LED blinking for STM8S105K4. I try to program it through ST-Link V2 adapter. But it shows warning as 'Warning : FILE : line 1: Address 0x4800 is out of range and is ignored!'.       I hav...

STM8 Bootloader enabling

Posted on June 19, 2016 at 14:54Hi all,I want to enable the STM8AF5289 bootloader for downloading the application through serial port. I have downloaded the ST visual programmer for this purpose .Can anyone please provide me the steps to be done for...

amitkrv22 by Associate II
  • 1072 Views
  • 0 replies
  • 0 kudos

CAN received message filtering mechanism

Posted on June 10, 2016 at 14:03Hi all,I am working on some CAN communication project which allows us to control some external device attached to one node from some other node.Since the CAn bus is a broadcast network and hence a message sent by a no...

amitkrv22 by Associate II
  • 1823 Views
  • 1 replies
  • 0 kudos

STDP6038

Posted on June 17, 2016 at 06:09Dear Sir, I am looking for a HDMI to LVDS controller chip From ST website I found that STDP6038 is the one of the controller chip. I want to interface laptop LCD screen to raspberry-pi via HDMI interface. I am attachi...

STM8L151F3 high failure rate

Posted on June 16, 2016 at 16:34Situation: Chip STM8L151F3U6.Circuit = MCU + LED (work time counter) After manual assembly, we have 80% of the output of defective products.Current consumption in reset from 0.1 mA to 8 mA (from sample to sample).Powe...

0690X00000602o3QAA.jpg

Small Device C Compiler 3.6.0 released

Posted on June 13, 2016 at 00:54Version 3.6.0 of SDCC, a C implementation targeting 8-bit architectures including the STM8 was released a few hours ago: Today a new release of SDCC was made. We are now at version 3.6.0. You can get it at: http://sou...

STM8L152R8 LCD Controller

Posted on June 12, 2016 at 05:43Hello,I'm currently working on STM8L152R8 and I need to drive a customized LCD glass. The problem is that I can not find any information about LCD_RAM[22:0] bits versus associated segments. For example I don't know wh...

Orcad and Viper06L Model

Posted on June 01, 2016 at 14:58Hello,I've a problem using the Viper06L Spice Model in Orcad 16.6 Lite. If I start the simulation I get the following error:ERROR(ORPSIM-15113): Model DZener used by X_U1.X_VIP06_CTRL_A1.X_X_OLF.D_D5 is undefinedYes I...

jens2399 by Associate II
  • 3974 Views
  • 8 replies
  • 0 kudos

Availability of previous Cosmic compiler versions?

Posted on December 04, 2015 at 12:05Hi thereWe've just come across a problem which may (not confirmed yet) relate to using a too-recent version of the Cosmic STM8 compiler. My binary works when compiled with 4.3.13, my colleague's does not when usin...

jro by Associate III
  • 2255 Views
  • 4 replies
  • 0 kudos

Different binaries on different machines

Posted on June 07, 2016 at 15:00We are facing issue to generate the binaries for our target microcontroller. The details/settings are as below.Microcontroller - STM8AF6246ST Visual Develop - version 4.3.9Cosmic compiler - version 7.5.1Memory model -...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.