Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8L ADC DMA issues

Posted on June 01, 2016 at 20:52Hi,    I am running my ADC in continuous mode to sample multiple channels multiple times.  I am using DMA to transfer the data to RAM in circular mode.  I am seeing occasional corruptions of individual samples.  I als...

stm8s003 ic

Posted on June 02, 2016 at 12:44Hi,I'm trying to use the ST Visual Develop with the Cosmic st8 32k compiler.  I install everything and build the project.  That all works fine.  When I try to connect to the Discovery board with the debugger using Swi...

stm8s003 ic

Posted on June 02, 2016 at 12:42while debug the program i got this error so please help me Emulator reset (usb://usb)...  ** Connection error (usb://usb): swim error [30200]: st-link connection error -> Failed to connect target.

Failing to build the project in STVD

Posted on May 31, 2016 at 08:15Hello,I am using STVD for STM8 project. I am facing a build error for 'param_assert' function. I am attaching the image for it. I tried including the file 'stm8s_conf.h' but still error persists. Can anyone help me res...

ssk by Associate II
  • 989 Views
  • 0 replies
  • 0 kudos

STM8S003 125khz PWM not work

Posted on May 29, 2016 at 11:50Hi All,I have new application used STM8S003, The MCU using timer1 or timer2 to generator 125khz PWM, duty cycle is 50% with 8Mhz HSI clock source.- This is my code to initial time2:static void Timer2_Init(void){ //Rese...

hungtp by Associate
  • 948 Views
  • 0 replies
  • 0 kudos

CANopen stack SPEAr320

Posted on September 14, 2011 at 10:13I'm looking for a CANopen software stack that can be implemented  with the BSP running under Linux on SPEAr320, for a project with a client  in the process automation. Any software available from ST or 3rd partie...

how to create library and hide its symbols

Posted on May 17, 2016 at 16:56Hi All.When using the STM 32f407 board.I want to create a library at keil uvision,based purely ANSI C.i just want the user to have an api h file and the library ,when i want all the library functions and variables (and...

haukeye by Associate II
  • 1298 Views
  • 1 replies
  • 0 kudos

Unable to clear I2C BUSY bit in STM8S-discovery

Posted on May 20, 2016 at 13:20 Unable to clear I2C BUSY bit in STM8S-discovery Hello Friends,  I have working experience of stm32f0xx microcontroller. But in case of stm8s003xx discovery board, I am stuck with a deadlock and am not able t...

raj by Associate
  • 813 Views
  • 0 replies
  • 0 kudos

Create I2C connection - STM8S103

Posted on May 18, 2016 at 17:34Hello forum,i am struggeling with the configuration of the I2C peripheral. Because there are literally NO tutorials out there how to do that i am asking here on this forum if anyone could give me a piece of code of how...

loder by Associate II
  • 759 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.