2015-12-04 3:05 AM
Hi there
We've just come across a problem which may (not confirmed yet) relate to using a too-recent version of the Cosmic STM8 compiler. My binary works when compiled with 4.3.13, my colleague's does not when using 4.4.2. I think these version numbers are correct, the various elements in use all have different numbers...Is there anywhere that 4.3.13 or other archive versions of the Cosmic compiler can be downloaded? I have a copy, but it would be reassuring if there was an archive on-line somewhere!If we figure out the cause of the problem I'll submit a bug report as appropriate.Best regardsJonathan2015-12-04 3:13 AM
2016-02-08 5:16 AM
I experencied the same trouble as Jonathan reported.
the case was: the same Sw, working perfectly when compiled by a colleague with Cosmic CXSTM8 v.4.3 included the the free package CXSTM8_EVAL, doesn't work when compiled with CXSTM8 v.4.4 included in the package CXSTM8 of 32K_Compilers suite. More in details the ''.s19'' first produced with v.4.3 is different from the other resulting from v.4.4 (the last 34 bytes in the program code and the const segment from 8000 to 8080, the target was STM8S003) After Installing v.4.3 of Cosmic and reconfigured STVD to the new compiler path, every other setting unchanged, the produced code is ok (and obviously the two binary are identical) Any idea of compatibility of the two version of Cosmic compilers ?2016-02-08 9:50 AM
2016-06-07 11:50 PM
Even we have also faced similar issue. It is undestood from Luca's update that it is generally normal. However, for us the differently generated binary fails to work, the software is not working the way it should.
Any idea on this?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.