Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BLDC Motor controller

I am new and novice can some one guide for using STM8Sxxx three-phase BLDC motor control software library V1.0. From the manual I am unable to build. Is there a tutorial or example on it. Looking for closed loop250W 36V Motor.

VSaha by Associate
  • 911 Views
  • 0 replies
  • 0 kudos

STM8AF6213PDU TIM5 and ADC1 library problem

I am using STM8AF6213 MCU in my project. I am using PD6 (AIN6) pin to read analog value. I use PD4 (TIM5_CH1) to generate PWM. But the stm8_adc1.h and stm8_tim5.h libraries that I included in my project do not work properly. It does not see the funct...

0693W000003QcmvQAC.jpg 0693W000003QcmlQAC.jpg
OOzde.2 by Associate
  • 759 Views
  • 0 replies
  • 1 kudos

Resolved! Impossible to re-open my old projects :

When I reimport the project from my PC or try to open it in the cloud. I have a short view to the design and next always the same question : "Sign in with your corportate ID" and then I can do nothing

PPito.1 by Associate II
  • 8161 Views
  • 11 replies
  • 0 kudos

What does the STM8 TIM3_BKRConfig() function do?

As a newbie I'm struggling to understand the following line of code:TIM3_BKRConfig(TIM3_OSSIState_Enable,TIM3_LockLevel_1,TIM3_BreakState_Enable,TIM3_BreakPolarity_High,TIM3_AutomaticOutput_Enable);Introductory material that I've found on timers/PWM ...

PiSquared by Associate II
  • 1535 Views
  • 1 replies
  • 0 kudos

Minimum supply voltage of M24M02

Hello,The minimum supply voltage for the M24M02 is 1.8 V (range of 1.8 V to 5.5 V). The Power Integrity Simulations ​of our hardware design showed a voltage of 1.7921 V @ pin A2 (VCC). This is a drop of almost 8 mV.I know, 8 mV below 1.8 V is almost ...

RAtem.1 by Associate
  • 1372 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.