2020-08-31 2:53 AM
Hello,
The minimum supply voltage for the M24M02 is 1.8 V (range of 1.8 V to 5.5 V). The Power Integrity Simulations of our hardware design showed a voltage of 1.7921 V @ pin A2 (VCC). This is a drop of almost 8 mV.
I know, 8 mV below 1.8 V is almost nothing, but will it work? Is it safe?
Best regards,
Roelof
2020-08-31 5:19 AM
Hello,
This is out of specification versus the guaranty granted by the datasheet. But you have to know that in order to guarantee the 1.8V operating, test pattern at EWS and Final Test are run at 1.7V. So even if lower than the Vcc min authorized, your die will work .
Best Regards
Team EEPROM suPPort
2020-08-31 6:22 AM
Hello,
Thank you very much for your answer.
Best regards,
Roelof
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.