Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem displaying numbers in 3 digits seven segment display interfaced with 74HC595 shift register? I am trying to send values from stm8s003f3 to display it in 3 digit seven segment display. I have interfaced Stm8s with 74hc595d for pin reduction.

The problem faced is that values send from controller is not displayed on 3 digit seven segment. I am attaching the program please tell me where i am doing wrong./* MAIN.C file *  * Copyright (c) 2002-2005 STMicroelectronics */#include "STM8s.h"void...

AMana.2 by Associate
  • 983 Views
  • 0 replies
  • 0 kudos

Debugger doesn't seem to be working

I have been following this tutorial:http://stm8sdiscovery.nano-age.co.uk/adventures-in-stm8-assembler/getting-started-with-the-blinking-led. When he does the "run to cursor" it stops on the instruction and highlights the editor window. Mine the out...

JTann.1 by Associate II
  • 1241 Views
  • 0 replies
  • 0 kudos

how to clear the pending external interrupt

@svlreg INTERRUPT_HANDLER(EXTI_PORTD_IRQHandler, 6){ /* In order to detect unexpected events during development,   it is recommended to set a breakpoint on the following instruction. */ if((SWITCH == RESET) && (flag == SET)) { OFF_STATUS = TRUE; fla...

Trinu by Associate III
  • 1368 Views
  • 0 replies
  • 0 kudos

STM8AF5286 UART3/LINUART not sending data

My following code is not working for sending data over LINUART port of STM8AF5286. I am using STVD and STM8_Standard_Project_Template.GPIO_Init(GPIOD, GPIO_PIN_5, GPIO_MODE_OUT_PP_HIGH_FAST);UART3_DeInit(); UART3_Init(9600,UART3_WORDLENGTH_8D,UART3_S...

PPate.1 by Associate III
  • 1720 Views
  • 2 replies
  • 0 kudos

Resolved! Is there a way for an STM8 MCU to determine programmatically if the SWIM interface is currently running?

Hi. Is there a way for an STM8 MCU to determine programmatically if the SWIM interface / ICP / STVD debugger are being used? I've tried checking the SWD bit in CFG->GCR and SWIM->CSR. But neither byte seems to change from SWIM debugging to a power on...

power draw when stopped STM8Lxxx

hi alli am first time user to ST micros. (8bit motorola mostly)I am looking at using stm8L132r8 in an ultra low power device, which needs 10year battery life.the micro will be stopped most of the time, woken by the RTC running from external 32khz xta...

dwood.1 by Associate
  • 763 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.