Problems running eDSim
Just installed eDSim 9.2 and on first run it stalls at 45% Looks like SIMetrix.exe is the problem. Tried running as admin, reinstalling without success. Suggestions?
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Just installed eDSim 9.2 and on first run it stalls at 45% Looks like SIMetrix.exe is the problem. Tried running as admin, reinstalling without success. Suggestions?
I hope you are well. I am working at C-DAC Bangalore, and I need guidance on using an ST-SAFE(STPM4RasPI) secure element / TPM module with a Python-based MQTT mTLS client on a Raspberry Pi. A short summary of our setup and goal: MQTT broker is alread...
Dear ST team, Please help to select controller for industrial automation. I have to design product for panel just to drive dc fan where the temperature high for cooling purpose.STM8 controller STM8S003F3P6, STM8S103F3T6, one of the controllers is sui...
Hi everyone,I recently purchased these chips they look original as the seller only sells genuine parts, but when I check them with a DMM, the Tab and pin 15 should have continuity these dont, Pin 15 and 8 should have continuity these dont. Can anyone...
I am trying to step into ST Microcontrollers. I have been able to blink LED of Blue Pill. My next attempt to interface 16x2 LCD with Blue Pill. An example code is being studied. In MikroC PIC Compiler control first goes to main() function from where...
Hi,Could you please confirm me the type of CRC16 used for data sent to a STSAFE-A110 chip? (CRC-A?, CRC-ARC?, CRC-CCITT?, ...)Thanks a lot.
Hello,given that the longevity commitment of the STM8 chips has been renewed for another 10 years, is an update planned for the old STVD development environment, which is no longer in line with other similar IDEs and also has some bugs? Sebastiano
Hardware / DT:I’m using ST M24M02DR (2 Mbit I²C EEPROM, page size 256 bytes, write cycle ~10 ms per byte/page) at 400 kHz. Device tree:eeprom@50 { compatible = "st,m24m02-dr", "atmel,24c2048"; reg = <0x50>; pagesize = <256>; num-ad...
Good afternoon everyone,I am currently working on a 1 kW Dual Active Bridge (DAB) converter with an input voltage range of 360 V–400 V and an output voltage range of 32 V–60 V. My objective is to design the converter with Zero-Voltage Switching (ZVS)...
Hello community,Can someone please assist to fix this issue in LTspice.Tried to add the spice model for SMA6T28CAY diode - Could not able to run the simulationAny suggestions? Best Regards,Vedanth
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.