Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stvp issue on win 10 when programing stm8

hello , i have an issue regarding stvp . before i used stvp on windows 7 and everything was working fine , but now i made an upgrade on windows 10 and it stops working. the error is ,,Cannot comunicate with the device .Check the swim cable .....'' If...

andrei17 by Associate
  • 689 Views
  • 2 replies
  • 0 kudos

Firmware Of Bridge less Pfc Circuit

I have an Queary ,How to design Firmware Of Bridge less Pfc Circuit ?For Below Specifiction input Voltage is varrible(Comes In AC) input current is constant (2.8 amps and 6.6amps )output voltage is constant 24vDCoutput Current Is 1.5AmpsNote : Input ...

nilmanivas_0-1765278369484.png

STA540 BTL parallel

Dear technical teamI'm designing a triamped system with the STA540 , in fact it uses two STA540's per unit.  I've divided the system in one STA amplifying stereo treble and mid, and other STA for bass amplifier, but given that bass channel is not ste...

nachus001_0-1757079172338.png
nachus001 by Associate II
  • 1423 Views
  • 1 replies
  • 0 kudos

Resolved! Programming PSD813F1A

We repair Fire Alarm Panels, and I have a known good chip PSD813F1A that I can read and save the data but when I program the blank device it will program but then gives me a verify error and it doesn't function in the panel. I'm using the Logical dev...

project with Ai-thinker Ra-09h

I have a project of making a point -2-point communication using lorawan protocol with the chip called AI-thinker Ra-09h that have an STM32WLE5 MCU . The problem is i dont have any knowledge in this field and i dont know how to deal with this module 

mazen29 by Associate
  • 449 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.