2025-11-25 1:16 AM - last edited on 2025-12-01 3:08 AM by Andrew Neil
2025-12-17 7:24 AM
Hi @PranavSangar,
Thanks for your interest in STSAFE-TPM solution.
One point to high is that the STSAFE-TPM is implementing TPM2.0 specification from TCG.
Therefore, STSAFE-TPM is compatible with TPM2.0 API.
That being said, to use a TPM in a Linux environment you will use several layers to achieve your goal.
In your context, the MQTT client relies on crypto library like OpenSSL.
In such case, you can check how to configure OpenSSL provider to use TPM (https://github.com/tpm2-software/tpm2-openssl).
To use the OpenSSL provider, you can configure it with openssl.cnf in the context of your MQTT client. In that case, the cryptography will be managed by the TPM provider.
Unfortunately, I don't have code snippet to provide you.
I have seen that paho-mqtt is using OpenSSL. This could be an interesting setup to explore.
Best Regards,
Benjamin
2025-12-19 4:18 AM
Hello,
Thank you for the suggestion.
I have already configured OpenSSL to use the TPM2 provider via openssl.cnf, so that cryptographic operations are handled by the TPM provider.
Below is the openssl.cnf file currently in use:
openssl_conf = openssl_init
[openssl_init]
providers = provider_sect
alg_section = algorithm_sect
[provider_sect]
default = default_sect
tpm2 = tpm2_sect
[default_sect]
activate = 1
[tpm2_sect]
module = /usr/local/lib/ossl-modules/tpm2.so
activate = 1
[algorithm_sect]
With this configuration:
OpenSSL successfully loads the tpm2 provider
Key operations work correctly when using TPM context files
However, the issue I am facing is specifically with using a TPM persistent handle (for example 0x81010001) in my MQTT client configuration.
When I try to reference the persistent handle (e.g. -key handle:0x81010001 or equivalent in the MQTT client), OpenSSL is not able to use the key, even though:
The handle exists in TPM (tpm2_getcap handles-persistent)
The same key works when referenced via a context file
So the problem is not provider loading, but persistent handle usage with OpenSSL + TPM2 provider in an MQTT/mTLS flow.
Could you please clarify:
Whether persistent handles are officially supported by the OpenSSL TPM2 provider for TLS client authentication
Or if only TPM context files are expected to be used with OpenSSL-based MQTT clients
Any guidance or reference documentation would be very helpful.
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.