Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

wakeup function

Please some one help me to how to get controller from sleep the configuration I made is not working.The below given code working fine and putting the controller in sleep but controller not waking up.The condition depends on mains (ADC Input channel 5...

SRAM.11 by Associate III
  • 1328 Views
  • 0 replies
  • 0 kudos

Storing Data in EEPROM on the STM8S003k3

Hi Everyone,I am using stm8s003k3 in one of my projects. I want to store a variable containing a  number from 0 to 999 in EEPROM but the issue is FLASH_ProgramByte & FLASH_ReadByte can only store a number up to 256. I tried to use FLASH_ProgramWord b...

KRiaz.1 by Associate II
  • 1854 Views
  • 1 replies
  • 0 kudos

Cannot connect to STM8S105 after setting ROP

I have been developing a project around the STM8S105 and I've been able to read and write the program and data memory fine several times (so I know that my STLink and dev board work well). Today I set the read-out protection to do some testing and af...

JSimo.6 by Associate
  • 2028 Views
  • 1 replies
  • 0 kudos

Why does Timer1 seem to have a slower clock?

I have a common function that I use to set up Timer 5 (I'm using it for PWM output, if it matters):timerCounts = CLK_GetClockFreq() / pow(2, TIM5_PRESALER_xx) / pwmFrequency;TIM5_TimeBaseInit(TIM5_PRESCALER_xx, timerCounts);And that works really well...

AWern.2 by Associate
  • 1582 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.