Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Currently the project in which I am working requires a precision of milliohms and we would like to have this value to carry out calculations.
HeyI have tried to use the option byte to stop the iwdg when i enter halt.I can see that i manage to set the WDG_HALTin option byte 3.But the watchdog still resets the MCU after i enter halt. Please help me, cant i do it? If so then how do i read tha...
My program is as described in stm8s reference manual 17.4.3 External clock source mode 1and pulse counting is done in pin PC7 using HSI 16 Mhz , but the speed of counting is very low , for example for a 10 mhz pulse in 1 ms TIM1_CNTRL counts to...
Hi,I am conducting research related to the change in thermal impedance during the failure of a SIC MOSFET, but I am finding it difficult to measure the same thermal impedance curve as in the datasheet when I start measuring. So I would like to ask ho...
Hello,I'am currently working on a implemented design out of the DesignStudio. The general purpose of the Viper26 in Buck Config is to supply another DCDC with 24V. Currently a load of 110 Ohm (Bleeder) Resistor is placed for testing purposes which re...
Hello Team I am using STVD IDE with cosmic compiler for development on STM8S207 series controller.I have two configurations in project called release and debug. whenever I try to debug code in debug configuration, following attached error appears whe...
We wanted to design 1kW traction motor controller for 3 phase BLDC motor., Therefore we were referring to this document found here.We tried generating the library with e STM8 MC FW builder and it worked fine. But these were only header file and no so...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.