Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! mcu gcc path

HiI need to modify many of the paths in the "project/c++/mcu gcc path". Is there a way to export/import the paths.Or are the paths in stored in a file so that i can edit that file directly ?I am trying to avoid to modify the paths one by one.The obje...

sgabran_0-1687839448800.png
sgabran by Associate III
  • 4131 Views
  • 2 replies
  • 2 kudos

STEVAL-STRKT01 dimension

Hello everybody!Wish y´all a good day, i´m considering to use the STRKT01 for a project but before i buy it i need to know the physical dimensions of the module/development card, also the dimensions of the case that the kit includes. Thanks! 

stm8s003f

Can someone please help me to sort it out?Please I am stuck at a project.In the attached code I am unable to wake up the code  after sleep.Rest of the functions working once in sleep it shoild wakeup at if(MV>20)#include "stm8s.h" #include "stm8s_clk...

SRAM.11 by Associate III
  • 1868 Views
  • 2 replies
  • 0 kudos

sleep and wake up

for my code the sleep and wake up is happening simultaneously I need  the wake up  only on if(MV>20) and sleep if(MV<100) for a minute(low power mode)Please someone help to sort it out #include "stm8s.h" #include "stm8s_clk.h" #include "stm8s_adc1.h"...

SRAM.11 by Associate III
  • 1590 Views
  • 0 replies
  • 0 kudos

Resolved! "Error : Programming failed" while trying to program "STM8S103F3" microcontroller with "STVP"

I got a message "Error : Programming failed" while trying to program "STM8S103F3" microcontroller with "ST visual Programmer". Sometimes the microcontroller got programmed but several times it failed. I am using "ST-LINK V2" programmer (connections: ...

STM8programmingfail.png

S2-LP Hardware Control

We are using S2-LP Transceiver to wireless products of us. Our custom board has 2 layer and 1.6mm thickness and our operating frequency(OP) is 868 MHz. Also our output power is 14dBmUnfortunately we failed "Unwanted Emission in Spurious Domain" test....

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.