2023-06-12 5:17 AM
Temperature range A = -40 °C to 85 °C and C = -40 °C to 125 °C
but ST72F561J9TBXS Datasheet not mentioned suffix B temperature range, could you please share? thanks!
2023-06-12 6:36 AM
Welcome, @Vivian Wang, to the community!
these particular microcontrollers were discontinued a long time ago, but were also not generally available, as they were custom devices that only the specific customer had documentation on.
There are also no substitutes for these devices.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter
2023-06-12 8:23 AM
Hi Peter, regarding ST72F561J9TAS suffix A means Temperature range A = -40 °C to 85 °C and C = -40 °C to 125 °C how about ST72F561J9TBXS ? Datasheet not mentioned suffix B temperature range, could you please share? thanks!
2023-06-12 8:28 AM
When a device is obsolete, I no longer have any support or documentation at all.
Sorry for not being able to help you in this case.
Regards,
/Peter
2023-06-12 10:26 AM
Thought TB was -40 to 125C, TA was -40 to 85C
The other more standard suffix method, ie
ST72F561AR9T6
Where 6 = -40 to 85C, 7 = -40 to 105C and 3 = -40 to 125C
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.