2024-05-07 10:23 PM - edited 2024-05-08 2:51 AM
hello,
i'm working on asm330lhh imu sensor and s32k324 nxp microcontroller.
Microcontroller : s32k324
imu sensor : ASM330LHH
interface : SPI
Question
1. i want to monitor vibration with this imu sensor. how can i implement code give me vibration monitor example code for asm330lhh. example code i checked but it is for ism330is sensor so i want for asm330lhh.
2. can i manullay implement code. if yes then what will be need i mean which parameters needs and what formulas to be need ?
2024-05-08 5:10 AM
You can look at the application note from ST for the IMU. On page 30, its outlined that the wake-up interrupt can be used. This is what you would need for a basic form of vibration detection.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.