MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DW12 celestial gravity

HelloIf a device using LIS2DW12 is fixed in a fixed position, will it be affected by the gravitational pull of the sun or moon and will the gravitational acceleration of each axis change?

meco by Associate II
  • 1734 Views
  • 2 replies
  • 0 kudos

Spikes in the LIS2DH12 accelerometer raw data

Spikes are present in the data coming from the LIS2DH12 accelerometer when placed in a casing, but when it is in the open there are no spikes. Attached is an image of the 3 axis data plotted from the accelerometer when placed on the table with casing...

Axis_Plot_closed_and_zreversed.png Axis_Plot_in_air.png

Comparison Between LSM6DS0 and LSM6DS3TR-C

Dear All,I hope this message finds you well.I am reaching out to inquire about the key differences between the LSM6DS0 and LSM6DS3TR-C sensors. Could anyone kindly provide insights into whether the LSM6DS3TR-C offers superior accuracy compared to the...

lis2dh12 configuration settings for the lowest power consumption

Are there any options to reduce the power consumption based upon the configuration I have set so far ?This while still being able to sample at 10Hz 10 bit and using FIFO so that the MCU could stay 'disabled' most of the time.For my project I need the...

Emiel by Associate II
  • 3625 Views
  • 5 replies
  • 2 kudos

lsm6DSO32XTR spi pin

Hi everyone,I'm working on setting up an SPI connection between the LSM6DS0x and an MCU. I'd like to clarify the pin configuration for a full-fledged SPI setup to ensure I'm getting the most accurate data.Specifically, I have the following questions:...

dhruvit by Associate II
  • 2223 Views
  • 1 replies
  • 0 kudos

LPS22HB LC_EN (low current mode enable)

Is there any application note or other information available about the LPS22HB's low current mode, as enabled by LC_EN in RES_CONF register? Other than reducing power consumption, what does it do and specifically, how does it affect performance?

tve by Associate II
  • 1615 Views
  • 2 replies
  • 0 kudos

IMU sensor

hello,i'm working on ASM330LHH imu sensor, right now i'm write code for gyroscope. when receving gyroscope data that time output is fluctuating without moving sensor, so how can stop this fluctuation please tell me procedure and most accqurate intili...

Detecting fast Z movement on LIS2DW12

Hello,I have code working well on the LIS2DH12 that I'm having trouble porting to a LIS2DW12. Unfortunately my new supplier only has boards with the LIS2DW12 and not the H12 so I have to port over my detection code to it. I have a sensor connected to...

nemik by Associate
  • 1518 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.