cancel
Showing results for 
Search instead for 
Did you mean: 

ST BLE Sensor App - Android - Sensor fusion

darla14
Senior

Does the ST BLE Sensor provided on github has the rotating cube code?

Do the inputs provided to the rotating cube is coming from the sensor-fusion running on the embedded device or on the App side?

Can you please point the code and the source files which is taking the input

Regards,

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Thanks for the reply,

I was checking this code of the firmware :

https://www.st.com/content/my_st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32-ode-function-pack-sw/fp-sns-motenvwb1.license=1629827087075.product=FP-SNS-MOTENVWB1.version=1.0.0.html

Here , the Quaternion characteristics are defined and I think here we are calling the below method to get the quaternions from the sensor fusion which is running in the Firmware ( STM32WB side) and then update the characteristics which are being received by the Classes you mention above in the App.

ComputeQuaternions >

 /* Run Sensor Fusion algorithm */

 MotionFX_manager_run(pdata_in, pdata_out, MOTIONFX_ENGINE_DELTATIME);

Quat_Update(MOTIONFX_Server_App_Context.quat_axes); > this then calls the  MOTENV_STM_App_Update_Char(MOTION_FX_CHAR_UUID, VALUE_LEN_QUAT, (uint8_t *)&value); which finally update the Quternion Charactertics and then it is being recieved by the App and Cube is rotated.

Please correct me !

Regards,

D

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.