MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST BLE Sensor App - Android - Sensor fusion

Does the ST BLE Sensor provided on github has the rotating cube code?Do the inputs provided to the rotating cube is coming from the sensor-fusion running on the embedded device or on the App side?Can you please point the code and the source files whi...

darla14 by Senior
  • 1496 Views
  • 2 replies
  • 0 kudos

Resolved! Tremendous problems in sourcing ST MEMS parts

We Ordered > 100k parts at the start of February this year: My distributor (EBV) is not even getting a confirmation date, and if something is given by ST, it is far in 2022. (Date today is August 13)ST, what is going on here? Please explain and infor...

MSimo.2 by Associate II
  • 3424 Views
  • 7 replies
  • 1 kudos

Resolved! I need to interface STM32 with SMI230 (Bosch's IMU sensor

Hello,I need to interface STM32 with SMI230 IMU sensor is there any libraries or driver for programming, I have found the linux driver for the SMI230, in my use case i am going to use STM32 MCU which cannot run linux OS, so "I need a driver which us...

BM.5 by Associate
  • 2128 Views
  • 1 replies
  • 0 kudos

LSM6DSO issues with I3C

LSM6DSO will NACK the broadcast after the RSTDAA sent in the reboot probe sequence.Here is the case to reproduce the issue:1. Only one LSM6DSO is on the I3C bus which is in pure I3C mode.2. The first-time kernel boot after power-up is okay. I3C bus a...

0693W00000D1F4WQAV.png

Resolved! LSM9DS1 motion detection functions

Hello! I tried to work with  motion detection function and here is my setup of interrupt pin /* Interrupt pin setup */ lsm9ds1_pin_notification_set(MAG_I2C_ADD, IMU_I2C_ADD, LSM9DS1_INT_PULSED); lsm9ds1_pin_polarity_set(MAG_I2C_ADD, IMU_I...

Zaren by Associate
  • 1478 Views
  • 1 replies
  • 0 kudos

There is a compile error in your VL32L1 code

vl53l1_class.cpp, Line 3864ff //Fix for some STM32 boards //Reinitialize th i2c bus with the default parameters#ifdef ARDUINO_ARCH_STM32 if (status) { dev_i2c->end(); // the method end() doesn't exist, you meant: dev_i2c->endTransm...

ritzeng by Associate II
  • 1192 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.