2014-02-12 8:13 PM
Hi, i have a problem with LSM330dlc.
Sometimes the gyroscope doesn't work fine. The gyroscope sends measures constants and then I should to disconnect the sensor of VCC (reset).After, in most cases it works well.With the accelerometer i don't have any problem.My code is (SPI communication):-------WriteSpiGiro(0x20,0xFF); // CTRL_REG1_G. Power ON: 760Hz; Cut-Off: 100Hz; X,y,Z axis: OnWriteSpiGiro(0x21,0x20); WriteSpiGiro(0x23,0x10);-------the other register are by default.is this particular sensor my problem? has this problem happened to someone else? thanks #lsm330dlc #gyroscopesWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.