2014-02-12 1:54 AM
I done I2c Communication with the LSM303DLM Module and am setting the normal power mode and ODR@50HZ and enabling xyz axises of Accelerometer and magnetometer and am reading the accelerometer and magnetometer readings but am getting 0's and 1's.How did aget data when sensor is in motion and changing directions. The following is the code i written to access the LSM registers.
Please any one help me to get dynamic data from the sensor. #define LSM_SDA PIN_C4 #define LSM_SCL PIN_C3 #use i2c(I2C2) int8 memxl,memxh,memyl,memyh,memzl,memzh,mxh,mxl,myh,myl,mzh,mzl; typedef short int i16_t; i16_t AXIS_X; i16_t AXIS_Y; i16_t AXIS_Z; i16_t M_AXIS_X; i16_t M_AXIS_Y; i16_t M_AXIS_Z; void LSM_INIT() { i2c_start(); //start i2c_write(0x30); // WR to LSM_A (SA0=0) i2c_write(0x20); // CTRL_REG1_A i2c_write(0x27); // data i2c_stop(); delay_ms(20); i2c_start(); i2c_write(0x30); // WR to LSM_A (SA0=0) i2c_write(0x28); //OUT_X_L_A i2c_start(); i2c_write(0x31); // RD from OUT_X_L_A memxl= i2c_read(0x28); // Read DATA i2c_stop(); i2c_start(); i2c_write(0x30); // WR to LSM i2c_write(0x29); // OUT_X_H_A i2c_start(); i2c_write(0x31); // RD from OUT_X_H_A memxh= i2c_read(0x29); // Read DATA i2c_stop(); AXIS_X = (i16_t)( (memxh << 8) | memxl ); i2c_start(); i2c_write(0x30); // WR to LSM i2c_write(0x2A); // OUT_Y_L_A i2c_start(); i2c_write(0x31); // RD from OUT_Y_L_A memyl= i2c_read(0x2A); // Read DATA i2c_stop(); i2c_start(); i2c_write(0x30); // WR to LSM i2c_write(0x2B); // OUT_Y_H_A i2c_start(); i2c_write(0x31); // RD from OUT_Y_H_A memyh= i2c_read(0x2B); // Read DATA i2c_stop(); AXIS_Y = (i16_t)( (memyh << 8) | memyl ); i2c_start(); i2c_write(0x30); // WR to LSM i2c_write(0x2C); // OUT_Z_L_A i2c_start(); i2c_write(0x31); // RD from OUT_Z_L_A memzl= i2c_read(0x2C); // Read DATA i2c_stop(); i2c_start(); i2c_write(0x30); // WR to LSM i2c_write(0x2D); // OUT_Z_H_A i2c_start(); i2c_write(0x31); // RD from OUT_Z_H_A memzh= i2c_read(0x2D); // Read DATA i2c_stop(); AXIS_Z = (i16_t)( (memzh << 8) | memzl ); i2c_start(); i2c_write(0x3C); // WR to LSM i2c_write(0x00); // CRA_REG_M i2c_write(0x00); // data i2c_stop(); i2c_start(); i2c_write(0x3C); // WR to LSM i2c_write(0x02); // MR_REG_M i2c_write(0x00); // data i2c_stop(); i2c_start(); i2c_write(0x3C); // WR to LSM-M i2c_write(0x03); // OUT_X_H_M i2c_start(); i2c_write(0x3D); // RD from OUT_X_H_M mxh= i2c_read(0x03); // Read DATA i2c_stop(); i2c_start(); i2c_write(0x3C); // WR to LSM i2c_write(0x04); // OUT_X_L_M i2c_start(); i2c_write(0x3D); // RD from OUT_X_L_M mxl= i2c_read(0x04); // Read DATA i2c_stop(); M_AXIS_X = (i16_t)( (mxh << 8) | mxl ); i2c_start(); i2c_write(0x3C); // WR to LSM-M i2c_write(0x05); // OUT_Y_H_M i2c_start(); i2c_write(0x3D); // RD from OUT_Y_H_M myh= i2c_read(0x05); // Read DATA i2c_stop(); i2c_start(); i2c_write(0x3C); // WR to LSM i2c_write(0x06); // OUT_Y_L_M i2c_start(); i2c_write(0x3D); // RD from OUT_Y_L_M myl= i2c_read(0x06); // Read DATA i2c_stop(); M_AXIS_Y = (i16_t)( (myh << 8) | myl ); i2c_start(); i2c_write(0x3C); // WR to LSM-M i2c_write(0x07); // OUT_Z_H_M i2c_start(); i2c_write(0x3D); // RD fromOUT_Z_H_M mzh= i2c_read(0x07); // Read DATA i2c_stop(); i2c_start(); i2c_write(0x3C); // WR to LSM i2c_write(0x08); // OUT_Z_L_M i2c_start(); i2c_write(0x3D); // RD from OUT_Z_L_M mzl= i2c_read(0x08); // Read DATA i2c_stop(); M_AXIS_Z = (i16_t)( (mzh << 8) | mzl ); fprintf(PC,''AX=%5d AY=%5d AZ=%5d MX=%5d MY=%5d MZ=%5d '',AXIS_X,AXIS_Y,AXIS_Z,M_AXIS_X,M_AXIS_Y,M_AXIS_Z); }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.