LSM330 vs LSM330DLC
Posted on January 27, 2014 at 07:06Hello, what is the difference between these two modules? Why DLC is so much expensive? #lsm330 #lsm330 #lsm330dlc
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Posted on January 27, 2014 at 07:06Hello, what is the difference between these two modules? Why DLC is so much expensive? #lsm330 #lsm330 #lsm330dlc
Posted on February 23, 2014 at 06:04The description page of the L3G4200D gyroscope says that it is an angular rate sensor able to provide unprecedented stablility of zero rate level and sensitivity over temperature and time. Does that mean that ther...
Posted on February 12, 2014 at 17:44HelloI am trying to use the LIS3DH in FIFO Mode with Filter enabled.In this mode, the X-Axis, and Y-Axis values get some normal values (they oscillate between -10 and +10) but the Z-Axis value seems to have a bypa...
Posted on December 16, 2013 at 14:53In LIS3DH datasheet (Doc ID 17530) on table 25 we can see: Default value 00 ODR3-0 (0000:50Hz Others:...) on table 26 we can see: 0000 Power down mode So what is ODR = 0000 Power down or 50Hz? #lis3dh
Posted on February 19, 2014 at 07:36Since there is a hole in the top of the LPS331APTR package, are special precautions needed during the assembly process? Is it OK to wash the boards?
Posted on February 18, 2014 at 16:40Not sure if this is the correct place to post this, but here we go. I'm considering using a pressure sensor to prototype a method for fuel level sensing. The sensor would be at the closed end of a straight tube ...
Posted on February 18, 2014 at 15:53Does anybody know if it possible to configure the LIS3DSH to apply a high-pass to the data output? #lis3dsh #high-pass
Posted on February 12, 2014 at 16:18What is the RF immunity of the ST MEMS microphones? How does the plastic package reject the radiated disturbances?
Posted on February 13, 2014 at 05:13Hi, i have a problem with LSM330dlc. Sometimes the gyroscope doesn't work fine. The gyroscope sends measures constants and then I should to disconnect the sensor of VCC (reset).After, in most cases it works well.W...
Posted on February 12, 2014 at 10:54I done I2c Communication with the LSM303DLM Module and am setting the normal power mode and ODR@50HZ and enabling xyz axises of Accelerometer and magnetometer and am reading the accelerometer and magnetometer read...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.