cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSOX/ISM330DHCX: real sample rate lower than expected in FIFO mode

GHope.2
Associate II

Hi,

I am using the LSM6DSOX and ISM330DHCX in FIFO mode at 52 Hz or 208 Hz. For 52 Hz the real frequency turns out to be about 48.57 Hz, and proportionally so for 208 Hz. I am confirming this through the number of samples collected between GPS fixes and when comparing a signal against another type of sensor. The observed frequency is stable at this rate.

Could this be real or is there something wrong in my application? The FIFO is checked using an RTC and is never allowed to run full (the overflow, full, overflow_latched) bits are checked. I drain (pop) the number of samples available at the RTC interrupt, but do not reset it. Does operating the FIFO or draining it halt the FIFO or reduce the number of samples?

I observe the same both with the LSM6DSOX and the ISM330DHCX.

IMU configuration: github.com/gauteh/sfy/blob/main/sfy-buoy/src/waves/mod.rs#L231

FIFO drain function: github.com/gauteh/sfy/blob/main/sfy-buoy/src/waves/mod.rs#L395

Best regards, Gaute

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @GHope.2​ ,

Welcome to ST Community!

You are not making any errors in your application, consider that the spread can span the +-10% range so having 48.57 Hz instead of 52Hz is acceptable.

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Federica Bossi
ST Employee

Hi @GHope.2​ ,

Welcome to ST Community!

You are not making any errors in your application, consider that the spread can span the +-10% range so having 48.57 Hz instead of 52Hz is acceptable.

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
GHope.2
Associate II

Thank you, that is a relief. Is the spread stable, i.e. will the frequency for an individual chip always remain the same? I've observed that a batch of instruments have apparently identical sample rate (48.57 Hz), but they may be from the same production batch. Is that still realistic?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.