Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hello,I'm testing LIS2DE12 accelerometer, trying to communicate with it through I2C. I want to make an interrupt on INT1 when some larger value is present (sensor is being shaken for example). I configured Interrupt to work on Or mode and for startin...
Please refer this thread. I don't think that the sensor can get damaged in such short period of time. Is it possibly due to moisture? At times I get 1018hPa which is even higher than sea level pressure of 1013.5 hPaPls help.
HI�?�?�?I came here to seek advice because I'm having trouble with the ISM330DHCX.I would like to calculate the maximum tolerance of the gyroscope sensor for an 8-year usage period of the ISM330DHCX based on the datasheet. Could you please guide m...
设置 ODR400HZ�?范围 2g�?�?�用 FIFO 并�?置�?模�?。读�?��?个寄存器的�?置没有问题。数�?��? 5 毫秒读�?�一次,FIFO �? time_ src=0x20 读�?�一次。
The library of VL53L4CX returns me a fatal error with the message no such file or directory, but the file it refers is in another directory of the same project. The project is just created and the error appears, can it be a bug or some problem with t...
Hi, I have created a machine learning model using STM32Cube IDE and would like to print out the results of the model on the PC using Bluetooth. I am using the SenorTile.box (STEVAL-MKSBOX1V1) with the SPBTLE-1S Bluetooth module.I am currently printin...
Motherboard: STEVAL-MKI109V3 (STM32F401VETX)IMU board: STEVAL-MKI197V (LSM6DSOX)Hello, I have ran into trouble setting the LSM6DSOX data rates of the XL and GY to 6667Hz in a custom STM32 project. The data is still fetched at a lower rate of around ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.