2018-10-18 2:47 AM
I try to use the LPS22HB as real pressure sensor (measure of force against the skin, but I almost didn't see any change. Only when press with big force I see the change.
Does the name of barometer mean it can't sense pure pressure against its window?
2018-10-22 5:35 AM
The pressure sensor sense air (or liquid in case of waterproof sensor) pressure.
There are holes in the window, through which the air is going to the sensing element.
2018-10-22 6:52 AM
Thanks Miroslav.
I understand why its not work for us.
Do you know on other MEMS or method we can measure true force ?
2018-10-23 1:54 AM
I read now about Piezoresistive MEMS LPS33HW. Also it is written as barometer,
2018-10-23 3:33 AM
measure true force with a strain gauge or load cell
they are cheap and linear
You can use a resistive touch screen if you are adventurous. (non trivial)
But these types of technologies have continual drift as stresses continually subside
and its a slow technology, readings every 500mS its a slow update speed.
2018-10-23 8:16 AM
@Barbie
I think you want to measure force, for that pressure sensor is not suitable.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.