MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3MDL not responding over SPI on custom PCB

Hi,I'm designing a flight controller pcb using several ST mems sensors, (LSM6DSO, LIS3MDL, LPS22HH) and interfacing them to an STM32H743IIT6 microcontroller over a shared SPI bus. I'm on the second iteration of this board, all sensors worked on the f...

VictorK_7-1725716130081.bmp VictorK_8-1725716140311.bmp VictorK_6-1725714206425.png VictorK_2-1725713533727.png
VictorK by Associate
  • 2671 Views
  • 2 replies
  • 2 kudos

Resolved! LIS2DE12 Tolerance

I am using a LIS2DE12 to detect when a mechanical shock occurs to my device. The datasheet provides only nominal values for the sample rate and the sensitivity.What is the tolerance on the sample frequency, I am using the ODR nominal rate of 5376 Hz?...

Resolved! How to select I2C on STEVAL-MKI109V

Hi All I am running Unicon GUI on Windows 10 and using it to communicate with STHS34PF80 sensor plugged onto STEVAL-MKI109V dev board.I can fully interact with the senor via the GUI app. Meaning reading and writing all registers of interest.I however...

ola by Associate III
  • 2047 Views
  • 4 replies
  • 0 kudos

LSM6DSV16X Gyroscope bias

Hi, I am currently evaluating the LSM6DSV16X IMU and I have a few questions regarding the sensor fusion functionalities, particularly the gyroscope bias.It is not very clear to me when to enable the gyroscope bias, and how to use the data it provides...

NicolasGoualard_0-1725228572664.png

Resolved! implement pedometer on ISM330IS

Hi all,we have a customer hardware with ISM330IS sensor on .We want to implement a pedometer on it like in the ISM330DHCX. Is it possible ?I followed the repo ism330is-pid/ism330is_reg.c at 413acfb51fd6f81a7449980a1caf286e37c909fe · STMicroelectronic...

apache by Associate II
  • 2795 Views
  • 5 replies
  • 1 kudos

Resolved! FSM_START_ADDRESS in LIS2DUX12

Hello,The LIS2DUX12 datasheet clearly states that "12.1.3 FSM_START_ADD_L (58h) and FSM_START_ADD_H (59h) FSM start address register (R/W). First available address is 0x35C.".The default address in MEMS-studio is 0x0200. In the FSM examples on GitHub...

zmogas by Associate II
  • 1295 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.