MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Run time fault detection in ASM330LHB

Hi,    I am using ASM330LHB in my project. ASM330LHB has only built self test which can only executed during power on to see ASM330LHB is healthy or faulty? But during runtime (device working in dynamic conditions) there is no way to find ASM330LHB i...

Pavani by Associate II
  • 1571 Views
  • 2 replies
  • 0 kudos

STHS34PF80 Abnormal operation

When STHS34PF80 detects the human body for a period of time, TPRESENCE cannot fall back normally, and pres_flag is always 1。 code:

top_0-1711014368016.png
top by Associate
  • 1947 Views
  • 3 replies
  • 0 kudos

LPS22DF Temperature compensation

Hi,I want to compensate for the temperature of the LPS22DF sensor.how does one go about programming for it? Is this formula correct?Pcorrected​=Pmeasured​−(TCF×(Tmeasured​−Treference​))If it is, should I use a temperature reference value of 25°C?Also...

nu by Associate
  • 849 Views
  • 0 replies
  • 0 kudos

Resolved! magnetometer Calibration Library does not work

Hello,    I am working on a custom board based on STM32F407 CPU with the LSM6DSV16XTR accelerometer+gyroscope and LIS2MDLTR magnetometer.The aim is to get board inclination and compass information with the maximum accuracy.The MotionFX library seems ...

MRaff.1 by Associate III
  • 3588 Views
  • 3 replies
  • 0 kudos

Resolved! LPS22DF I3C addressing

Dear forum,We plan to assemble five LPS22DF sensors on the same I3C bus and (off course) to address them individually. According to the datasheet (7.4.1 MIPI I3CSM CCC supported commands) the answer to GETPID can only have two values, depending on SD...

tcachat by Associate II
  • 1877 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.