cancel
Showing results for 
Search instead for 
Did you mean: 

Run time fault detection in ASM330LHB

Pavani
Associate II

Hi,

    I am using ASM330LHB in my project. ASM330LHB has only built self test which can only executed during power on to see ASM330LHB is healthy or faulty? But during runtime (device working in dynamic conditions) there is no way to find ASM330LHB is healthy or faulty?

1. Please suggest a method to find ASM330LHB is healthy or faulty during runtime?

2. Is ASM330LHB is fully calibrated against over its temperature range?

Thanks in advance,

Pavani.

 

 

2 REPLIES 2
Federica Bossi
ST Employee

Hi @Pavani ,

The self test works only in static conditions.

I confirm that ASM330LHB is calibrated over the entire temperature range.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi, Thank you for your reply. How many times we can perform self test (in static condition) for ASM330 in its lifetime? Is there any limit OR can we perform self test unlimited times? If there is any limit please mention the count.

Thanks in Advance,

Pavani

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.