MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SSC architecture driver

Hi,Our customer is integrating LSM6DSM and LSM6DS3TR sensors with QCM2150 platform and stuck in production. This requires Qualcomm SSC architecture driver and configuration for LSM6DSM and LSM6DS3TR , so that we can integrate it into ADSP firmware.Co...

BluenrgM2sp module connection regarding

After programming bluenrgm2sp module it is not discoverable in the ST BLE-scanner.I have used the bluenrg2 navigator code.Please help me to find the solution.Thank you in advance.

Applied by Associate
  • 1044 Views
  • 0 replies
  • 0 kudos

Regarding the LSM6DSO IMU

I am using NRF5340 board for development using the LSM6DSO IMU sensor.Is there any way so that I can write a particular value inside the LSM6DSO sensor in non-volatile form. Please let me if it is possible.Please let me know as soon as possible.

LSM9DS0 accelerometer issues

Back in 2015, I ordered 19 LSM9DS0 boards from Adafruit for a project (which is taking longer than anticipated!).I've recently noticed that the Accel X, Y and Z readings are materially different for some boards when the boards are flat in a common po...

LSM303AGR using only temperature sensor

Hello,I'd like to use LSM303AGR temperature sensor and only that, what is the minimal configuration to be able to do that? As I browsed the forum I saw that setting TEMP_EN[1:0] bits to 1 in the TEMP_CFG_REG_A and BDU bit in CTRL_REG4_A is not enough...

jjay by Associate
  • 1449 Views
  • 2 replies
  • 0 kudos

QVAR Sensor - LSM6DSV16X

Is it possible to check the electrical activity of an AC power cable using Qvar functionality. What type of electrode to be used? What type of input circuitry needs to be designed (input impedance and filtering)?   

marshouse by Associate II
  • 1708 Views
  • 2 replies
  • 0 kudos

Resolved! Access to calculated features for LSM6DSOX

I guess this is a weird question. I am not really interested in the classifying part of the MLC but I am interested in its feature selection capability, I would like to know if it is possible to perform feature extraction calculation on the data sto...

WGeng.1 by Associate II
  • 2542 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.