2024-10-24 11:18 AM - edited 2024-10-29 9:27 AM
Is it possible to check the electrical activity of an AC power cable using Qvar functionality.
What type of electrode to be used? What type of input circuitry needs to be designed (input impedance and filtering)?
2024-10-24 12:04 PM
Yes, it's possible to detect electrical activity in an AC power cable noninvasively using Qvar functionality as described in ST's AN5755. The Qvar sensor can sense electrostatic charge variations when electrodes are placed near the cable's outer insulation. The electrodes, typically made of conductive material, should be placed close but not touching the cable.
For the input circuitry, high impedance (megaohms range) is required to prevent signal interference, along with filtering to eliminate noise, focusing on the AC signal's frequency (50/60 Hz)
2024-10-24 12:25 PM - edited 2024-10-29 9:27 AM
Is there any criteria for dimensions of the foil that matters for this use-case?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.