MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ASM330LHH can not updata regiter

... I'm using ASM330LHH chip, I'm using the SPI communication method, when I initialize the write to these registers, I confirm that it has been written, I go to read the STATUS_REG register, and I find that it has always been 0, and then I go to rea...

c458f9db14cea4493516f41adac62ed.png 9ab966ea38871e179c5eeffa9fdf29d.png
doudou by Associate II
  • 1806 Views
  • 2 replies
  • 0 kudos

My sensor tile box not responding yet all

 Hello All,My new sensor tile box STB011147 not responding yet all even connected USB power source to it's not responding, I checked the battery was connected, however when I pressed power button no LED are turning on. please let me know how to resol...

vkosuri by Associate III
  • 1891 Views
  • 1 replies
  • 0 kudos

Reading data from STEVAL_MKI197V1 via STEVAL_MKI109V3

How would I go about reading data from gyroscope and accelerometer of lsm6dsox IMU in the STEVAL_MKI197V1 that is connected to PC via STEVAL_MKI109V3 motherboard WITHOUT the need to use software like Unico-GUI?  Preferably I would like to have the da...

MartinR by Associate
  • 1251 Views
  • 1 replies
  • 0 kudos

Resolved! Information about gyro sensor in LSM6DSO32

What is the type of internal (mechanical) structure of LSM6DSO32 gyro sensor? (a photo of the internal structure would be beneficial). The reviewer asked us about this during the review process, and we couldn't find such information in the manual. Be...

DominikS by Associate
  • 1188 Views
  • 1 replies
  • 1 kudos

STWIN.box starter kit periodic data logging

Hi,I have a STWIN.box starter kit and would like to use it for solar powered periodic vibration (IIS3DWB) data logging into an SD card. What would be the easyest way to do this?For example datalog vibration for 2 minutes every hour into the SD card.R...

iarakis by Associate II
  • 1030 Views
  • 1 replies
  • 0 kudos

X-NUCLEO-IKS01A3 code

Hi, Can you help me to use the LSM6DS0 sensor in the IKS01A3 board with the nucleo f767ZIThanks

RF by Associate II
  • 9730 Views
  • 5 replies
  • 0 kudos

MEMS studio - board support

hi. I attended a workshop a few weeks ago and had no difficulties using MEMs studio with my X-NUCLEO-IKS4A1.  I needed to move to a new computer and I went through the download process again for MEMS studio and my board (above) is not shown as suppor...

Rauscher by Associate II
  • 1705 Views
  • 2 replies
  • 2 kudos

Resolved! Code for STEVAL-MKI109V3 with STEVAL-MKI210V2K

Good morning,I'm using the STEVAL-MKI109V3 board associated with the STEVAL-MKI201V2.Is there a source code for using the STEVAL-MKI201V2 accelerometer with the STEVAL-MKI109V3 board?Otherwise there are examples of using the STEVAL-MKI201V2 with othe...

Gb2 by Associate II
  • 2117 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.