MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What does position signify in linux sysfs for LIS331DLH

Posted on March 04, 2014 at 17:58 There is a linux sysfs file for accessing data from LIS331DLH. cat /sys/devices/platform/lis3lv02d/position What does this actually retrieve. Cartesian co-ordinates? If yes, with respect to what...

kiran by Associate
  • 650 Views
  • 0 replies
  • 0 kudos

Gyro LPF1 in LSM330DLC

Posted on March 03, 2014 at 22:56There is  a low pass filters LPF1 which is after ADC(page 22 of the data sheet Doc ID 022162 Rev 2 ).There is no words about this filter can anybody tell me a bit more about it? for example what is the cut off freque...

haxyan by Associate
  • 655 Views
  • 0 replies
  • 0 kudos

Measuring Dynamic acceleration using LIS2DH

Posted on March 03, 2014 at 08:43I have calculated Tilt/Gradient in Non-accelerated systems(System acceleration  = 0); How to measure Tilt/Gradient in accelerated systems.As MEMS will give the X,Y,Z component of the resultant acceleration(g and a )....

LIS3DH impact detection

Posted on March 01, 2014 at 10:23HelloI have read that impact detection functionality can be performed by LIS3DH. I am unable to find any information on HOW to configure the device for impact detection.Is it identical to ''click'' detection? If no -...

igor2 by Associate II
  • 724 Views
  • 0 replies
  • 0 kudos

LSM9DS0 +16g range

Posted on February 26, 2014 at 11:06I've set up the LSM9DS0 to the +/-16g range by setting AFS2 - 0 as 100 as per datasheet. Normal g comes out as 0.7g, yet all other ranges are fine. What am I doing wrong? Chris

clock stability, and sampling rate on LSM9DS0

Posted on October 26, 2013 at 09:15There are no figures for clock stability over time and temperature. These are going to effect the sample rate times. For example, if the accelerometer DOR is 100Hz, what spread can be expected. I take it that in al...

Configuring LIS3DH

Posted on February 20, 2014 at 08:31I connected LIS3DH in the following way , but the device does'nt give the correct reading.          What is wrong with this configuration? Vin = 3.3V, SPI 4 wires. I configured the registers with the following str...

yohai by Associate
  • 1830 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.