MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LISDH12 high consumption

Posted on November 03, 2016 at 17:34Hi all,i use an accelerometer  LISDH12, and it have a very high consumption (400 uA).I have this configuration; SCL/SDA connect to vdd with 4.7kCS to high because i want to use a i2cSDA0 put on groundSomeone hav...

anna by Associate
  • 1144 Views
  • 3 replies
  • 0 kudos

MKI109V2 motherboard firmware upgrade

Posted on November 09, 2016 at 20:03Hi,I just got new MKI109V2 motherboard, and installed the driver for DFU and VCP. At the beginning, I can detect VCP on my PC and use DFU DEMO to upgrade firmware. After upgrading firmware DFU_Patcher_V1.0.2.dfu, ...

ljin by Associate
  • 1047 Views
  • 1 replies
  • 0 kudos

LSM303AGR Acclerometer jerk detection

Posted on November 06, 2016 at 07:50Hi I am planning on using LSM303AGR to detect a jerk in my system. And I want LSM303AGR to send an INT1 to the CPU to wake.I am thinking to use the accelerometer to determine this jerk. Magnetometer will be in sle...

toashwin by Associate
  • 870 Views
  • 0 replies
  • 0 kudos

LSM303AGR Arduino based Examples

Posted on November 06, 2016 at 07:43HiI am thinking of using LSM303AGR I2C interface. Are there any Arduino based examples for this product?I could not find any online.Thanks #arduino

toashwin by Associate
  • 708 Views
  • 0 replies
  • 0 kudos

LSM303AGR or LSM303DLHC - which one more sensitive e-Compass?

Posted on November 06, 2016 at 07:33Hi From the spec I see, LSM303DLHC has magnetic range as 8.1g. And LSM303AGR as 50g.So what does that mean? Which one more sensitive? which one more accurate?Does that mean, unless there is a big delta in magnetis...

toashwin by Associate
  • 1056 Views
  • 0 replies
  • 0 kudos

LSM6DS3 Problem with interrupts

Posted on November 03, 2016 at 01:31So as in title I'm having problem in configuring LSM6DS3 to send DRDY on INT1 and INT2 lines. Basically I wan't to have drdy of acc on int1 and drdy of gyro on int2. However after writing to both INT1 and INT2 reg...

ChrisH by Associate III
  • 690 Views
  • 1 replies
  • 0 kudos

LIS3DHTR ''noisy'' output

Posted on November 01, 2016 at 10:14I'm trying to get an LIS3DH accelerometer working and I have a question about the output data.It seems to be very ''noisy''. I have the board with the accelerometer on a flat table.I've set the data rate to 100hz ...

Rob1 by Associate II
  • 951 Views
  • 1 replies
  • 0 kudos

LPS22HB in aerodynamic

Posted on November 01, 2016 at 12:14Hi,I want to use LPS22HB to measure the pressure on some points of a wing profile.Is it possible if I build the right embodiment?Rocco #lps22hb

API timeout in VL53L0X_get_info_from_device()

Posted on October 27, 2016 at 03:57I have modified the platform.h and platform.c to run on Raspberry Pi.  The i2c-tools show I can read the device, and the routine VL53L0X_DataInit() returns no error, so I can write to the device.  But I am getting ...

mrosing by Associate II
  • 3002 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.